DDR3L chips for LS1021A new designs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR3L chips for LS1021A new designs

Jump to solution
1,206 Views
fzhang
Contributor II

Trying to use the same DDR3L devices on the TWR-LS1021A-PB board for LS1021A, but they (MT41K256M16HA-125:E) are obsoleted.  

Found this one on digi-key which is the closest model (higher clock speed rating but slightly smaller package):

http://www.digikey.com/product-detail/en/micron-technology-inc/MT41K256M16TW-107-XIT-P/557-1757-ND/6...

I think this one should work with the memory controller on LS1021A without any schematic changes from the TWR-LS1021A-PB board. But I need the confirmation from NXP experts so that I can move ahead with this DDR3L on my new board.

If there is better options please also let me know, I'd really appreciate it.

Labels (1)
Tags (1)
0 Kudos
1 Solution
1,010 Views
ufedor
NXP Employee
NXP Employee

> MT41K256M16TW-107 but at a "lower speed rate -- 800MHz", right?

Yes, it will work the same way as with MT41K256M16HA.

> And one last question, do the driver or settings and configurations need to be updated to work with this DDR3L?

No.

View solution in original post

0 Kudos
3 Replies
1,010 Views
ufedor
NXP Employee
NXP Employee

According to the Micron datasheet the main difference is a package (HA vs TW).

0 Kudos
1,010 Views
fzhang
Contributor II

Thank you, ufedor,

The memory controller on LS1021A should work with

MT41K256M16TW-107 but at a "lower speed rate -- 800MHz", right?

And one last question, do the driver or settings and configurations in Linux need to be updated to work with this DDR3L?

Thanks,

0 Kudos
1,011 Views
ufedor
NXP Employee
NXP Employee

> MT41K256M16TW-107 but at a "lower speed rate -- 800MHz", right?

Yes, it will work the same way as with MT41K256M16HA.

> And one last question, do the driver or settings and configurations need to be updated to work with this DDR3L?

No.

0 Kudos