Hello,
I am designing custom board using LS1012A processor and interface with two 1Gx8 DDR3L micron DDR3L chip.
During layout, I am facing issue of routing of data lines so that as per AN3940 (Hardware and Layout Design 
Considerations for DDR3 SDRAM Memory Interfaces) I have swapped the datalines in D0 to D7 at first DDR3L end.
Also, attached swapped connections of first DDR3L with Processor.
So, will it work for me? because I can't see any information or guide to change this bits from firmware configuration level and confusion on the connections.
Looking for your help.
It is possible to swap bits within a byte lane.
Please refer to the AN3940, Table 1. DDR3 Designer Checklist, 45:
https://www.nxp.com/webapp/Download?colCode=AN3940
Note that the MMDC supports only x16 data bus width.