DDR test on LS1021A in u-boot or kernel without codewarrior/jtag

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DDR test on LS1021A in u-boot or kernel without codewarrior/jtag

跳至解决方案
1,534 次查看
winstonjacob
Contributor IV

I am using LS1021A custom board, we need to do the DDR test with the temperature  -40C to +80C inside thermal chamber, please suggest me to  the DDR test in u-boot or kernel without codewarrior or the jtag.

 

Regards

Winston.

0 项奖励
回复
1 解答
1,524 次查看
Pavel
NXP Employee
NXP Employee

Use the "mtest" command from u-boot for memory testing. See the following page:

https://github.com/ARM-software/u-boot/blob/master/doc/README.memory-test

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,525 次查看
Pavel
NXP Employee
NXP Employee

Use the "mtest" command from u-boot for memory testing. See the following page:

https://github.com/ARM-software/u-boot/blob/master/doc/README.memory-test

0 项奖励
回复