DDR test on LS1021A in u-boot or kernel without codewarrior/jtag

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR test on LS1021A in u-boot or kernel without codewarrior/jtag

ソリューションへジャンプ
1,505件の閲覧回数
winstonjacob
Contributor IV

I am using LS1021A custom board, we need to do the DDR test with the temperature  -40C to +80C inside thermal chamber, please suggest me to  the DDR test in u-boot or kernel without codewarrior or the jtag.

 

Regards

Winston.

0 件の賞賛
返信
1 解決策
1,495件の閲覧回数
Pavel
NXP Employee
NXP Employee

Use the "mtest" command from u-boot for memory testing. See the following page:

https://github.com/ARM-software/u-boot/blob/master/doc/README.memory-test

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,496件の閲覧回数
Pavel
NXP Employee
NXP Employee

Use the "mtest" command from u-boot for memory testing. See the following page:

https://github.com/ARM-software/u-boot/blob/master/doc/README.memory-test

0 件の賞賛
返信