DDR test on LS1021A in u-boot or kernel without codewarrior/jtag

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR test on LS1021A in u-boot or kernel without codewarrior/jtag

Jump to solution
1,512 Views
winstonjacob
Contributor IV

I am using LS1021A custom board, we need to do the DDR test with the temperature  -40C to +80C inside thermal chamber, please suggest me to  the DDR test in u-boot or kernel without codewarrior or the jtag.

 

Regards

Winston.

0 Kudos
Reply
1 Solution
1,502 Views
Pavel
NXP Employee
NXP Employee

Use the "mtest" command from u-boot for memory testing. See the following page:

https://github.com/ARM-software/u-boot/blob/master/doc/README.memory-test

View solution in original post

0 Kudos
Reply
1 Reply
1,503 Views
Pavel
NXP Employee
NXP Employee

Use the "mtest" command from u-boot for memory testing. See the following page:

https://github.com/ARM-software/u-boot/blob/master/doc/README.memory-test

0 Kudos
Reply