DDR read/write issues custom board LS1046A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR read/write issues custom board LS1046A

11,727 Views
Rinke
Contributor II

Hi all,

 

I am in the process of trying to bring up a LS1046A board. Its a custom board based heavily off the Freeway design. The first step I am trying to do is get the connection diagnostics to pass with RCW override and DDR settings. D_INIT is cleared and its gets to the DDR memory access test. However when checking logs I can see that the DDR values do not match their expected values. See picture and logs(Read_Write_mem.txt). I see some resemblance of the expected values. D_Init_value is set to 0xDEADBEEF. 

 
 

Screenshot 2025-02-03 214119.png

Some things we tried and validated:

Hardware:

- Schematics reviewed and double checked

- Voltages are checked. GVDD, VREF, VTT and VPP

- Input and output DDR clocks

- DRAM reset signal is correct

- MEM enable signal is correct

Software:

- RCW correct and double checked. See below

- DQS skews are correct and double checked with schematics

- DQ mapping should be correct. Using the exact same layout as the Freeway board. See attached. 

 

Screenshot 2025-02-03 214611.png

I am unable to find a DDR config for the Freeway board. Is this something we can get to compare to our settings? Any pointers to what might be wrong? Im assuming its settings related since D_INIT is cleared and we are actually able to read/write to DDR. 

You can also find the logs below for the test for centering the clocks. Its ran with RCW override with the RCW mentioned below. CCS Output is also added. 

 

 

RCW:

RCWSR1:0x0810000d
RCWSR2:0x0a000000
RCWSR3:0x00000000
RCWSR4:0x00000000
RCWSR5:0x00000000
RCWSR6:0x40000002
RCWSR7:0x40000000
RCWSR8:0xc1000000
RCWSR9:0x00000000
RCWSR10:0x00000000
RCWSR11:0x00000000
RCWSR12:0x00000800
RCWSR13:0x00000000
RCWSR14:0x00000000
RCWSR15:0x00000096
RCWSR16:0x00000001

 

Any tips and/or pointers to potential fixes is appreciated. 

 

Rinke

0 Kudos
Reply
25 Replies

1,568 Views
yipingwang
NXP TechSupport
NXP TechSupport

DDRv tool doesn't use the DDR parameters coming from the firmware deployed on the target board. Please ignore atf software.

When starting the validation, DDRv tool will reset the target board and configure the target board according to the parameters filed in DDRv tool properties panel.

So you need to modify "properties" panel according to your DDR datasheet.

If your problem persists, would you please capture CCS console and error log in QCVS DDRv tool IDE?

0 Kudos
Reply

1,559 Views
Rinke
Contributor II
I wiill make a new topic to discuss the current issues. Since the issue this topic is about was solved.
0 Kudos
Reply

1,414 Views
valokuvaaja
Contributor II
@Rinke Do you have any updates? We have almost the same problems with our custom LS1046A board.
0 Kudos
Reply

1,396 Views
Rinke
Contributor II

Hi,

Nope, we keep getting bits set in the F04 debug register. And NXP does not explain what they mean. But their software does checks on this register. We are seeking external help. Since NXP support doesnt really seem interested in helping.

0 Kudos
Reply

2,974 Views
Rinke
Contributor II

Hereby the initialization file