Hi,
I have a TWR-LS1021a eva board and with linux 4.19 kernel
when I ran dbus on this device I always encountered this error below: any one knows why?
$2 = (gchar *) 0xb2c05668 "GDBus.Error:org.freedesktop.DBus.Error.ServiceUnknown: The name org.XXXXX.server was not provided by any .service files"
this is the debug statement from the gdb
I did previously fix the error regarding "Failed to open connection to "session" message bus: Unable to autolaunch a dbus-daemon without a $DISPLAY for X11"
Hello Elias Bitbaker,
What rootfs filesystem are you using?
Please refer to the following log when I run lsdk1909 rootfs filesystem.
root@localhost:/mnt/bin# /mnt/etc/init.d/dbus start
* Starting system message bus dbus
...done.
root@localhost:/mnt/bin# ps aux | grep dbus
message+ 534 0.0 0.2 5744 2936 ? Ss Jun30 0:00 /usr/bin/dbus-daemon --system --address=systemd: --nofork --nopidfile --systemd-activation --syslog-only
message+ 26503 0.0 0.2 5612 2244 ? Ss 19:02 0:00 /usr/bin/dbus-daemon --system
root 26524 0.0 0.0 2124 492 ttyS0 S+ 19:03 0:00 grep --color=auto dbus
Would you please provide your console log including Linux Kernel booting up and all your operations under Linux?
Thanks,
Yiping
Hi Yiping,
The dbus is running now previously is due to a configure file under /etc/dbus-1/system.d/ needs to assign root permission to the policy user.
However, current issue is the CPU usage reaches 190% high every time while running my application on d-bus wonder if you have any suggestions to debug this?
===============================================
root@localhost:/etc/dbus-1/system.d# [ 1118.654731] Out of memory: Kill process 649 (demo-server) score 886 or sacrifice child
[ 1118.662690] Killed process 649 (demo-server) total-vm:1024472kB, anon-rss:905288kB, file-rss:0kB, shmem-rss:0kB
===============================================
root@localhost:/etc/dbus-1/system.d# ps aux | grep dbus
message+ 269 0.4 0.3 5992 3084 ? Ss 12:37 0:00 /usr/bin/dbus-daemon --system --address=systemd: --nofork --nopidfile --systemd-activation --syslog-only
root 545 0.0 0.0 2120 532 ttyS0 S+ 12:40 0:00 grep --color=auto dbus
===============================================