Cross compile with gdb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cross compile with gdb

Jump to solution
3,295 Views
bladerunner1010
Contributor III

which toolchain should I use?

0 Kudos
Reply
1 Solution
3,270 Views
Pavel
NXP Employee
NXP Employee

LSDK recommends the following toolchain:

gcc-linaro-4.9-2016.02-x86_64_aarch64-linux-gnu–

 

See LSDK User Guide.

https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev20.12.pdf

View solution in original post

0 Kudos
Reply
3 Replies
3,282 Views
Pavel
NXP Employee
NXP Employee

1. NXP offers LSDK 2108 for the LS1043ARDB board:https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/layerscap... See the Chapter 4.1.9 in LSDK 2108 User Guides:https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev21.08.pdf This Chapter contains documentation for building and deploying LSDK on the LS1043a board. LSDK 2108 recommends using the following toolchain:

gcc-linaro-4.9-2016.02-x86_64_aarch64-linux-gnu– Used to compile UEFI firmware (can be downloaded from: https://releases.linaro.org/components/toolchain/binaries/4.9-2016.02/aarch64-linuxgnu/gcclinaro-4.9...)

0 Kudos
Reply
3,288 Views
bladerunner1010
Contributor III

which toolchain?

 

0 Kudos
Reply
3,271 Views
Pavel
NXP Employee
NXP Employee

LSDK recommends the following toolchain:

gcc-linaro-4.9-2016.02-x86_64_aarch64-linux-gnu–

 

See LSDK User Guide.

https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev20.12.pdf

0 Kudos
Reply