Hello to all, my goal is to get my LS1043a board to boot by SD and starting the system by shutting down cores 1, 2 and 3. Once the system is up and running, i would like to see from uboot that such cores are disabled.
I performed a custom boot in which I entered the PBI command to disable the cores.
The procedure I followed is well described and can be found in the following link: Procedure
I'm starting u-boot, and then so far so good.
But to make sure that the cores are off I went to read the DCFG_CCSR_COREDISR register, at the address 1EE_0094h using the following u-boot command:
md 0x1ee0094 1
The result I get is the following:
0x1ee0094: 0x0e000000
I shouldn't be reading instead:
0x1ee0094: 0x0000000e
since in the datasheet the bits of that register are defined in this way:
已解决! 转到解答。