Coming out of the Asleep mode in LS1028ARDB

cancel
Showing results for 
Search instead for 
Did you mean: 

Coming out of the Asleep mode in LS1028ARDB

280 Views
sameer_chouksey
Contributor II

Hello everyone,

I am using LS1028ARDB switch for some applications. The switch is working fine except sometimes when it goes to asleep mode. The D25 LED will turn ON and will be on all the time. I tried resetting and restarting the device but still the device is not coming out of the asleep mode. 

Can someone please help me with the procedure to bring the device out of the asleep mode?

Thanks & Regards,

Sameer 

#ls1028#tsn; ls1028;time sensitive networking#tsn#asleep led‌ #asleep

0 Kudos
3 Replies

216 Views
ufedor
NXP TechSupport
NXP TechSupport

Please provide U-Boot and Linux booting log as textual attachment.

0 Kudos

216 Views
sameer_chouksey
Contributor II

I am not able to access the board when in SD boot. As soon as I power it on LED D25 turns yellow and the power button SW1 also turns yellow. I don't see any thing on the teraterm. 

The only time D25 turns off and the power button SW1 is not yellow is when I change SW2 to eMMC boot mode. I am attaching the logs when it is in eMMC boot. 

Regards,

Sameer  

Logs:

-------------------------------------------------------------------------------------------------------

U-Boot SPL 2018.03-00132-g5dea3b77e7-dirty (Dec 05 2018 - 22:52:53 +0530)
Initializing DDR....
WARNING: Calling __hwconfig without a buffer and before environment is ready
WARNING: Calling __hwconfig without a buffer and before environment is ready
WARNING: Calling __hwconfig without a buffer and before environment is ready
WARNING: Calling __hwconfig without a buffer and before environment is ready
Trying to boot from MMC1


U-Boot 2018.03-00132-g5dea3b77e7-dirty (Dec 05 2018 - 22:52:53 +0530)

SoC: LS1028AE Rev1.0 (0x870b0010)
Clock Configuration:
CPU0(A72):1300 MHz CPU1(A72):1300 MHz
Bus: 400 MHz DDR: 1600 MT/s
Reset Configuration Word (RCW):
00000000: 34004010 00000030 00000000 00000000
00000010: 00000000 00bf0000 0030c000 00000000
00000020: 00a03150 00002580 00000000 00002496
00000030: 00000000 00000010 00000000 00000000
00000040: 00000000 00000000 00000000 00000000
00000050: 00000000 00000000 00000000 00000000
00000060: 00000000 00000000 2006705a 00000000
00000070: bb580000 00000000
Model: NXP Layerscape 1028a RDB Board
Board: LS1028A-RDB, Board Arch: V0, Board version: C, boot from eMMC card
FPGA: v6.0
SERDES1 Reference : Clock1 = 100.00MHz Clock2 = 100.00MHz
I2C: ready
DRAM: 3.9 GiB
DDR 3.9 GiB (DDR4, 32-bit, CL=11, ECC on)
"Error" handler, esr 0xbf000002
elr: 0000000096042420 lr : 00000000960020a0 (reloc)
elr: 00000000fbdaa420 lr : 00000000fbd6a0a0
x0 : 0000000020400000 x1 : 0000000000000000
x2 : 00000000d00dfeed x3 : 0000000001e00210
x4 : 0000000001e00214 x5 : 00000000000011a0
x6 : 0000000000001168 x7 : 0000000000000002
x8 : 0000000000001164 x9 : 000000000000000c
x10: 00000000fbb6193c x11: 00000000fbb61a88
x12: 0000000000001168 x13: 00000000fbb6199c
x14: 00000000fbb61a88 x15: 00000000fbb619ac
x16: 0000000000000001 x17: 0000000000000000
x18: 00000000fbb63d88 x19: 0000000020400000
x20: 00000000fbdd2968 x21: 0000000065d68000
x22: 000000001801deb1 x23: 0000000018009dd8
x24: 000000001801de99 x25: 0000000018020000
x26: 00000000deadbeef x27: 0000000001e00404
x28: 0000000001e00210 x29: 00000000fbb61960

Resetting CPU ...

### ERROR ### Please RESET the board ###

0 Kudos

216 Views
ufedor
NXP TechSupport
NXP TechSupport

Please verify that there is bootable firmware on the inserted SD card.

Use pre-built composite firmware images available at:

LSDK Open Source 

section LSDK IMAGES

0 Kudos