Can SGMI(2.5) be connected to 2500Base-x in ls1043a?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can SGMI(2.5) be connected to 2500Base-x in ls1043a?

跳至解决方案
398 次查看
lijun10210
Contributor III

The SGMII(2.5G) mode of ls1043 is connected to AQR115C 2500base-x.

My status is:PHY link is ok,but  the ping and PHY  loopback tests are fail。

I don't know why it's like this, is it because SGMII(2.5G) and 2500base-x are incompatible?

Hope for your answer,thanks a lot。

0 项奖励
回复
1 解答
386 次查看
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @lijun10210,

Please refer to section# 33.2.1 mentioned in LS1043ARM in which the supported features are mentioned.

Regards,
Mrudang

在原帖中查看解决方案

0 项奖励
回复
1 回复
387 次查看
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @lijun10210,

Please refer to section# 33.2.1 mentioned in LS1043ARM in which the supported features are mentioned.

Regards,
Mrudang

0 项奖励
回复