Can I use CodeWarrior USB TAP/ CWH-UTP-PPCC-HE for QorIQ LS1012ARDB ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use CodeWarrior USB TAP/ CWH-UTP-PPCC-HE for QorIQ LS1012ARDB ?

883 Views
changwonson
Contributor I

this is the revisited case of the previously opened case:00100814(Opened on :1/13/2017).
The LS1012ARDB's debug console port does not work.
As NXP support advised, we tried to replace the board.
But, the local resailer refused the process.

Now, I need to reinstall the firmware of the console/downloader.

What I need to be assisted are:

1. can I use the CodeWarrior USB TAP/CWH-UTP-PPCC-HE to
   reinstall firmware for either K22/TAG or ls1012A/JTAG?
   - ls1012A JTAG is 1.8v logic and CWH-UTP-PPCC-HE is 3.3v

2. Which JTAG need to be used K22/TAG or ls1012A/JTAG?
  
3. Where can I find the bin file to resolve the problem?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

721 Views
ufedor
NXP Employee
NXP Employee

Please create a Technical Case:

https://community.freescale.com/thread/381898

0 Kudos
Reply