Booting ls1021atwr SDK 1.9 u-boot image from SD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Booting ls1021atwr SDK 1.9 u-boot image from SD

Jump to solution
2,418 Views
MatthiasFuchs
Contributor II

Hi,

I am trying to boot u-boot from sd card on a ls1021atwr board.

The board states: SCH-28040 REV D1. I expect this board to have a silicon 1.0 CPU installed.

I finally need QSPI support so I am using this binary image from the SDK 1.9 under ls1021atwr:

-r-xr-xr-x 1 root root   547488 Dec  3 15:16 u-boot-sdcard-qspi-2015.01+fslgit-r0.bin*

lr-xr-xr-x 1 root root       40 Dec  3 15:16 u-boot-sdcard-qspi.bin -> u-boot-sdcard-qspi-2015.01+fslgit-r0.bin*

The image is written to SD card as follows:

#~ sudo dd if=<above image> of=/dev/sdX bs=512 seek=8

DIP switches are setup as follows:

SW2: 00100111

SW3: 01100001

I do not get a single character on the serial console.

Does the SDK 1.9 support my CPU silicon? If not, is there still support for this silicon in the used U-Boot sources?

Matthias

Labels (1)
0 Kudos
1 Solution
1,564 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Matthias Fuchs,

SDK 1.9 doesn't support LS1021 1.0 CPU, it is used for 2.0 CPU.

For LS1021 1.0 CPU, please download QorIQ SDK 1.8 from https://nxp.flexnetoperations.com/control/frse/product?child_plneID=684021&cert_num=181474981&ver=AR...​.

You could refer to a similar thread from SDcard boot SDK 1.8 LS1021a .


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
4 Replies
1,565 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Matthias Fuchs,

SDK 1.9 doesn't support LS1021 1.0 CPU, it is used for 2.0 CPU.

For LS1021 1.0 CPU, please download QorIQ SDK 1.8 from https://nxp.flexnetoperations.com/control/frse/product?child_plneID=684021&cert_num=181474981&ver=AR...​.

You could refer to a similar thread from SDcard boot SDK 1.8 LS1021a .


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,564 Views
PLE
Contributor II

Hello Yiping Wang,

When you say "SDK 1.9 doesn't support LS1021 1.0 CPU", is that also for Linux kernel ? Or only Uboot as Matthias Fuchs asked ?

I mean, can we use Linux source from SDK 1.9 with Uboot from SDK 1.8 or 1.7 on LS1021A rev 1 board ?

Thanks

Philippe

0 Kudos
1,565 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Philippe,

It's better to use u-boot and Linux Kernel from the same SDK.

Thanks,

Yiping

0 Kudos
1,565 Views
janbrand
Contributor II

Hello,

is there a difference between the schematic of Tower-Board SCH-28040 REV D1 and newer ones? In detail I mean the connection between Lanes and Ethernet-PHYs? (see in pics added to this post). We've bought the SCH-28040 REV D1 board. Is it possible then to use SDK 1.8?

kind regards,

Jan Brand

0 Kudos