Are there PCIe bandwidth numbers vs packet size available for the LS1021A as a root complex?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are there PCIe bandwidth numbers vs packet size available for the LS1021A as a root complex?

1,099 Views
Larry5335
Contributor IV

Are there PCIe bandwidth numbers vs packet size available for the LS1021A as a root complex?

Labels (1)
0 Kudos
Reply
1 Reply

905 Views
alexander_yakov
NXP Employee
NXP Employee

I do not see LS1021A PCIe bandwidth benchmarking numbers ready to share. Please consult our Sales/Marketing team for the question if these benchmarks may be performed per your request.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply