Add Second MMC to LS1021A Device Tree

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Add Second MMC to LS1021A Device Tree

489件の閲覧回数
Kensou
Contributor III

Hello Everybody,

I would like to add a second eMMC in LS1021A with custom Buildroot Linux image and device tree for a custom board based on LS1021A-IOT board (with additional eMMC, of course).

Using Buildroot I am able to modify and customize the Linux Image.

What is the correct manner for adding additional peripherals? 

0 件の賞賛
1 返信

462件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

LS1021A only has one esdhc controller, it is impossible to use a second MMC.

You could replace the SD interface with eMMC.

0 件の賞賛