About the terminator of DDR3L memory of LS1020A.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About the terminator of DDR3L memory of LS1020A.

1,345件の閲覧回数
masaakiuno
Contributor I

Hello,

I am watching a connection diagram of LS1021A-twr.

A terminating resistance of CLK of DDR3 of P1010RDB is just between± 100 Ω.

LS1021A-twr adds a condenser to 72 Ω of resistance, and is connected to GVDD.

Is this circuit the specification of LS102xA? Or is there a different reason?

In particular, I can't understand the reason that a condenser exists by this circuit.

Best Regards,

Maaski.Uno

ラベル(1)
0 件の賞賛
返信
1 返信

1,259件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please note that it is not convenient to create several threads for a single issue.

Let's communicate through the About the terminator of DDR3L memory of LS1020A.

0 件の賞賛
返信