About the terminator of DDR3L memory of LS1020A.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About the terminator of DDR3L memory of LS1020A.

1,269 次查看
masaakiuno
Contributor I

Hello,

I am watching a connection diagram of LS1021A-twr.

A terminating resistance of CLK of DDR3 of P1010RDB is just between± 100 Ω.

LS1021A-twr adds a condenser to 72 Ω of resistance, and is connected to GVDD.

Is this circuit the specification of LS102xA? Or is there a different reason?

In particular, I can't understand the reason that a condenser exists by this circuit.

Best Regards,

Maaski.Uno

标签 (1)
0 项奖励
回复
1 回复

1,183 次查看
ufedor
NXP Employee
NXP Employee

Please note that it is not convenient to create several threads for a single issue.

Let's communicate through the About the terminator of DDR3L memory of LS1020A.

0 项奖励
回复