About LS1043ARDB EVM 10G PHY

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About LS1043ARDB EVM 10G PHY

633 Views
gyosunshim
Contributor III

Hi all,

I am testing with the LS1043ARDB-PB EVM board.
The AQR105-B1 has SPI Flash (MX25V4006E) memory,
It seems that 10G PHY does not work when memory is removed.
Do I need to write data to SPI Flash?
How can I write if I need to?
Is it possible on u-boot?

Thank you.
Best regards,

gyosun.

Labels (1)
Tags (1)
0 Kudos
1 Reply

505 Views
Pavel
NXP Employee
NXP Employee

Is FMAN microcode loaded on your board?

Look at the Section 4.4.7.4 of the SDK 2.0-1703 Documentation:

http://www.nxp.com/assets/documents/data/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos