4K resolution is not supported on ls1028ardb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

4K resolution is not supported on ls1028ardb

Jump to solution
1,430 Views
Eddy1
Contributor IV

Hi:

Does ls1028ardb support 4K resolution? When the 4K resolution is set, it is found that the Weston desktop is not displayed. The steps are as follows:

1.vi /etc/xdg/weston/weston.ini:

idle-time=0
#use-g2d=1
#xwayland=true
gbm-format=argb8888

[libinput]
#touchscreen_calibrator=true

[output]
name=DP-1
mode=3840x2160@60
force-on=true
#transform=90

[shell]
size=3840x2160

2.Then set the Weston display:

root@LS1028ARDB:~# mkdir -p /run/user/0/
root@LS1028ARDB:~# export XDG_RUNTIME_DIR="/run/user/0/"
root@LS1028ARDB:~# weston --tty=1 &

3.check the mode

root@LS1028ARDB:~# weston-info

04:37:42.155] failed to create input devices
[04:37:42.171] DRM: head 'DP-1' found, connector 56 is connected, EDID make 'AOC', model 'U2790R3B', serial '7010'
[04:37:42.179] Registered plugin API 'weston_drm_output_api_v1' of size 24
[04:37:42.221] Chosen EGL config details: id: 51 rgba: 8 8 8 8 buf: 32 dep: 0 stcl: 0 int: 1-60 type: win|pix|pbf|swap_preserved vis_id: ARGB8888 (0x34325241)
[04:37:42.221] Output DP-1 (crtc 48) video modes:
3840x2160@60.0, preferred, current, 533.2 MHz

I would appreciate your advice?

0 Kudos
1 Solution
1,403 Views
Pavel
NXP Employee
NXP Employee

Besides the steps you listed, the following steps are needed for 4K resolution.
1. Update the bootargs in uboot and change it to 4K as attached log.
2. apply the patch as attched.

View solution in original post

0 Kudos
2 Replies
1,404 Views
Pavel
NXP Employee
NXP Employee

Besides the steps you listed, the following steps are needed for 4K resolution.
1. Update the bootargs in uboot and change it to 4K as attached log.
2. apply the patch as attched.

0 Kudos
1,307 Views
Eddy1
Contributor IV

Thank you very much for your support.

0 Kudos