Hi,
Am working on LS1046ardb Kit. I am able configure all the four 1G Ports of LS1046ardb kit i.e. set ipaddress and netmask. When i try to ping the ports , I get reply only from one out of the four ports for all the ipadress - all the ports are in the same network. But I get reply from respective ports when i set them in different network.
I want to work in same network. Kindly Help.
You could configure route table to bind the source IP address to the specific Ethernet port.
# ip r add 100.1.1.100 dev eth2
# ip r add 100.1.1.101 dev eth3
# ip r
100.1.1.100 dev eth2
100.1.1.101 dev eth3