16-bit QSPI chip with LS1046A-based board

取消
显示结果 
搜索替代 
您的意思是: 
已解决

16-bit QSPI chip with LS1046A-based board

跳至解决方案
685 次查看
JRRandall
Contributor III

Hi,

We have a 16-bit QSPI chip we are trying to use as the boot device for our LS1046A-based board.  We noticed in the LS1046A FRWY initialization PBI commands there is a command that looks like it's setting the QuadSPI_MCR to 64-bit LE (write 0x550000, 0x000f400c).

Questions:

Are we able to use 16-bit QuadSPI on with the LS1046A? It looks like all the NXP designs use 8-bit QSPI, which is probably compatible with switching the endianness like this.

Will a 16-bit QSPI be able to endian swap on the qspi controller?

标签 (1)
0 项奖励
1 解答
680 次查看
ufedor
NXP Employee
NXP Employee

QSPI controller endianness is configured for internal data exchange and is independent of the connected SPI device.

在原帖中查看解决方案

0 项奖励
1 回复
681 次查看
ufedor
NXP Employee
NXP Employee

QSPI controller endianness is configured for internal data exchange and is independent of the connected SPI device.

0 项奖励