如何通过eno0 ssh登陆LSDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

如何通过eno0 ssh登陆LSDK

696 Views
s8113595
Contributor I

LSDK系统通过串口配置eno0后,能ping通主机。但是主机不能通过eno0 ssh登录系统? 请问要如何才能通过eno0 ssh登陆系统呢?

pastedImage_1.png

0 Kudos
Reply
1 Reply

620 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello li shaoyong,

It seems that sshd server process on your target board is not set up, please check whether sshd is running with the following command.

root@localhost:~# ps aux | grep sshd
root 3767 0.0 0.1 10412 5020 ? Ss 15:58 0:00 /usr/sbin/sshd -D
root 4778 0.0 0.0 2708 440 ttyS0 S+ 16:07 0:00 grep --color=auto sshd

If no, please generate Ubuntu rootfs filesystem with the following command in LSDK.

$ flex-builder -i mkrfs -r ubuntu:main

For details, please refer to the section "LSDK userland" in LSDK 19.09 document.

Thanks,

Yiping

0 Kudos
Reply