When customer’s ethernet PCS could not link up, this article will give a guide how to debug it step by step based on the T1024.
Many ethernet is configured by the SerDes, so how to confirm the link error is caused by the SerDes or the PCS itself. This article will give some clues.
Serdes Lane&pins
First check which SerDes lane the you are using, please confirm the SerDes land in the QorIQ T1024 Reference Manual. Such as configuration below, the user case set the SRDS_PRCTL_S1=0x05B in the RCW[128:136], the application will utilize the SGMII.m1 and SGMII.m2.
01.png
fmacaddress.png
This article will consider SGMII.m1 as an user case, now the SGMII will in the Frame Manager, MAC1.
Check the SerDes Lane Assignments to confirm the Lane of the SerDes, for the SGMII.m1, the specific lane pins name would be SD1_TX3P/N and SD1_RX3P/N. it could be recognized as Lane 3.
MAC number is not related to the Serdes lane number, should confirm the specific table to get the pins.
lane.png
Any hardware test with this ethernet should related the pins, see the component pin number below.
pins.png
You could test the eye diagram of RX pins of this Lane to confirm if the frequency is correct. if you set this Lane to SGMII 1.25G, you could confirm the speed is set correctly by the eye diagram.
eyediagram.png
Eye diagram above, just show the speed of the SerDes.
That is very important when loopback correctly, but could to connect to other device.
How to confirm the SerDes link up
Please find the Lane register in the QorIQ T1024 Reference Manual.
In this user case it’s Lane 3, so should read out the Lane 3 registers to confirm if the SerDes Lane 3 work well. Such as below:
# Lane 3
md.l 0xFFE0EA8C0 1 - aa611080 # LN3GCR0
md.l 0xFFE0EA8C4 1 - 101c4019 # LN3GCR1
md.l 0xFFE0EA8CC 1 - 00002800 # LN3SSCR0
md.l 0xFFE0EA8D0 1 - 0f0fc01f # LN3RECR0
md.l 0xFFE0EA8D4 1 - 0f0f0fa8 # LN3RECR1
md.l 0xFFE0EA8D8 1 - 00003006 # LN3TECR0
md.l 0xFFE0EA8E0 1 - 39000400 # LN3TTLCR0
md.l 0xFFE0EA8E4 1 - 00000000 # LN3TTLCR1
md.l 0xFFE0EA8F4 1 - 00000000 # LN3TCSR1
md.l 0xFFE0EA8FC 1 - 04000000 # LN3TCSR3
SerDes_LNnTCSR3 is an important debug test register, the CDR_LCK is to check if the CDR locked or not.
CDR_LCK=0 means a valid bit stream is not detected. As a test, you could put the lane in loopback mode LN2TCSR3[LPBK_EN]=01. The CDR should lock in digital loopback mode (internal loopback). If not, there could be an issue with the device itself.
So, if you could set the LPBK-EN to “01” Loopback Mode, it will set the SerDes’s own TX and RX signals in Loopback Mode to exclude external signals, then check the CDR_LCK again, if it’s 1, then SerDes itself works well. Anyway, CDR_LCK should always be set.
In the “md.l 0xFFE0EA8FC 1 - 04000000 # LN3TCSR3”, the CDR_LCK=0, suspect the SerDes level issue.
The normal status should be:
=> md fe0ea8fc 1
fe0ea8fc: 08000000
CDR.png
How to confirm the PCS link up
The MAC and PHY registers should get the details from the T1024DPAArm, QorIQ T1024 Data Path Acceleration Architecture (DPAA) Reference Manual
Find the offset address in the DPAARM.
FMAC2.png
For the SGMII MAC address should be offset+0x1000.
Follow the 6.5.4 MDIO Ethernet Management Interface usage in the T1024DPAARM to read the MDIO registers.
In this application, SGMII1, MAC1, you could find the MAC1 address would be FM1_mEMAC1: 4E_0000, so FM1_mEMAC1 MDIO registers would be 4E_1000h.
In the user case, the protocol is SGMII, should follow the 6.5.4.3 Clause 22 Read Flow in the T1024DPAARM.
6.5.4.3 Clause 22 Read Flow
1) Wait for MDIO_CFG[BSY] = 0.
2) Write MDIO_CTL with proper PHY_ADDR and REGISTER_ADDR and with bit 16 set.
3) Wait for MDIO_CFG[BSY] = 0.
4) If the addressed PHY did not respond then MDIO_CFG[MDIO_RD_ER] is set.
Otherwise read MDIO_DATA value.
In this user case, should read the MDIO_SGMII_SR, you could find the register definition in the QorIQ T1024 Reference Manual, 30.5.5 1000Base-KX PCS MDIO Memory Map/Register Definition
The key bits would below:
STATUSREG.png
STATUSREG2.png
Here the user case result:
When you read MDIO_SGMII_SR, please use manual input that can meet the delay time requirement.
If you could not input manually, please follow the flow, " Wait for MDIO_CFG[BSY] = 0" before read MDIO_DATA value.
Read SGMII1 MDIO Registers
=== Serdes Test 1 ===
0xFFE0EA8FC value: 0x08000000
Dump PCS0 Registers 0xFFE4E1030-0xFFE4E103C:
0x40001408
0x00000000
0x00001340
0x00001340
Select 0x8002 ,devmem 0xFFE4E1034 32 0x8002
Read: 0x00000083
Select 0x8003 ,devmem 0xFFE4E1034 32 0x8003
Read: 0x0000E400
Select 0x8001 ,devmem 0xFFE4E1034 32 0x8001
Serdes0 Status: 0x00000029
Select 0x8001 devmem 0xFFE4E1034 32 0x8001
Serdes0 Status: 0x0000002D
Select 0x8001, devmem 0xFFE4E1034 32 0x8001
Serdes0 Status: 0x0000002D
The first time, it’s not link, LINK_STAT is 0(0x00000029), and then it’s turn to 1(0x0000002D).
Now the PCS link up and the HW loopback checking is completely.
View full article