Prerequisites: The board should be running Linux and connected to terminal console. 
 Note: For log level debug support, the restool version should be LSDK-2003-RC1 or above and MC version should be 10.20.0 or above. 
 To check restool version: 
 $ root@localhost:~# restool -v
restool LSDK-20.04
 
 To check MC version: 
 root@localhost:~# restool -m
MC firmware version: 10.24.0
 
 For debugging, use the ls-debug script available in the LSDK rootfs. There is no need to create the debug object. 
 ls-debug -h  
  ls-debug options 
 
 
 -h, --help 
 ls-debug help information 
 
 
 -ts, --timestamp=X 
 Enable/Disable timestamp printing, X is ON or OFF 
 
 
 -c, --console=X 
 Enable/Disable printing in UART console, X is ON or OFF 
 
 
 -l, --log=X 
 Enable/Disable printing in DDR log, X is ON or OF 
 
 
 -u, --uart=X 
 Set UART ID of the console, X = [0 - 4], 0 = OFF 
 
 
 -ll, --level=X 
 
 Set logging level, X = [0 - 5] 
 
 0: Global 
 1: Debug 
 2: Info 
 3: Warning 
 4: Error 
 5: Critical 
 
 
 
 
 -m, mem, --memory 
 
 Dump information about memory modules available 
 
 
 
 dpxy.z 
 
 Dump information about MC respective object 
 
 
 
 
   
 For example, to enable logging in console with log level INFO: 
 $ ls-debug --log=on --console=on --level=2              
dpdbg.0 created
DDR log printing ON
UART console printing ON
Log level set to 2
$ root@localhost:~# ls-debug --memory
Memory dumped information available in MC log/console
$ root@localhost:~# cat `find /dev/ -name "*mc_console"`
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_get_obj for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dpdbg_open on DPDBG
[I, RESMAN]  Handling command: dpdbg_dump on DPDBG
[I, DPNI]  Memory info:
[I, DPNI]  MC DDR #1 cacheable memory
[I, DPNI]        Total: 134217728 bytes
[I, DPNI]        Used: 14802708 bytes
[I, DPNI]        Free: 119415020 bytes
[I, DPNI]  MC DDR #1 non-cacheable memory
[I, DPNI]        Total: 50331648 bytes
[I, DPNI]        Used: 27680 bytes
[I, DPNI]        Free: 50303968 bytes
[I, DPNI]  DMEM1 memory
[I, DPNI]        Total: 81920 bytes
[I, DPNI]        Used: 27168 bytes
[I, DPNI]        Free: 54752 bytes
[I, DPNI]  DMEM2 memory
[I, DPNI]        Total: 81920 bytes
[I, DPNI]        Used: 27168 bytes
[I, DPNI]        Free: 54752 bytes
[I, DPNI]  DDR #1 memory
[I, DPNI]        Total: 1610612736 bytes
[I, DPNI]        Used: 143163392 bytes
[I, DPNI]        Free: 1467449344 bytes
[I, DPNI]  PEB memory
[I, DPNI]        Total: 2097152 bytes
[I, DPNI]        Used: 524288 bytes
[I, DPNI]        Free: 1572864 bytes
[I, DPNI]  DP-DDR memory
[I, DPNI]        Total: 4294967296 bytes
[I, DPNI]        Used: 0 bytes
[I, DPNI]        Free: 4294967296 bytes
[I, RESMAN]  Handling command: dpdbg_close on DPDBG
[I, RESMAN]  Handling command: dprc_close for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_set_irq_mask for DPRC 1 on portal id 0
[I, RESMAN]  Handling command: dprc_set_irq_enable for DPRC 1 on portal id 0
root@localhost:~#
  
        
        查看全文