Does any support for Aquantia AQR108 in LS1043A ?
Should be add below patch, but I don't know AQR108's device id.
Need to check spec.
+
+struct phy_driver aqr108_driver = {
+ .name = "Aquantia AQR108",
+ .uid = 0x3a1????, <- Need to check spec
+ .mask = 0xfffffff0,
+ .features = PHY_10G_FEATURES,
+ .mmds = (MDIO_MMD_PMAPMD | MDIO_MMD_PCS|
+ MDIO_MMD_PHYXS | MDIO_MMD_AN |
+ MDIO_MMD_VEND1),
+ .config = &aquantia_config,
+ .startup = &aquantia_startup,
+ .shutdown = &gen10g_shutdown,
+};
+
int phy_aquantia_init(void)
{
phy_register(&aq1202_driver);
phy_register(&aq2104_driver);
phy_register(&aqr105_driver);
+ phy_register(&aqr108_driver);
return 0;
}
Thanks a lot! We have the datasheet of AQC108 ethernet controll with PCI express. Unfortunately, we can't find out any information about the .uid. Any keyword we can use to know the correct uid ?