Packet Forwarding Engine (PFE) Ethernet Ports Setting up on LS1012A Platform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Packet Forwarding Engine (PFE) Ethernet Ports Setting up on LS1012A Platform

Packet Forwarding Engine (PFE) Ethernet Ports Setting up on LS1012A Platform

LS1012A integrates a hardware packet forwarding engine to provide high performance Ethernet interfaces. This document introduces PFE hardware and software decomposition and data flow, setting up two PFE Ethernet ports to implement Ethernet packets forwarding through PFE, how to modify PFE driver and dts file to set up single PFE Ethernet port on LS1012A custom boards.

PFE hardware Structure

PFE Software Decomposition and Data Flow

Setting up Two PFE Ethernet Ports to Implement Ethernet Packets Forwarding

Set up Single PFE Ethernet Port on LS1012A Custom Boards

Labels (1)
Attachments
100% helpful (1/1)
Version history
Last update:
‎10-09-2017 06:06 PM
Updated by: