In the U-Boot log, the names of the Ethernet interfaces are printed in the format <name>@<interface type>, for example, DPMAC3@xgmii. DPMAC is a DPAA2 object that identifies the physical interface.
Interface name is not fixed in LX2160ARDB, depending upon which interface is active, name will be assigned in TinyDistro as well as in Ubuntu distribution.
Interface names can be checked using ls-listni command.
root@TinyDistro:~# ls-listni
dprc.1/dpni.1 (interface: eth0, end point: dpmac.2)
dprc.1/dpni.0 (interface: eth1, end point: dpmac.17)
For details regarding creation of a DPAA2 network interface (DPNI) in Linux, see "LSDK Quick Start Guide for LX2160ARDB -> Bringing up DPAA2 network interfaces" in Layerscape Software Development Kit User Guide.
The table below shows the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux for LX2160ARDB.
| Port name on chassis |
Port name in U-Boot |
Port name in Linux (tinyDistro) |
Port name in Linux (Ubuntu userland) |
Description |
| 40G MAC2 |
DPMAC2@xlaui4 |
Interface name will be ethn, for example eth0, eth1. Eth0: If PCIe is connected, else it is any connected DPAA2 interface. |
PCIe: enp1s0
DPAA: ethx
|
40G MAC2 QSFP+ port |
| 10G MAC3 |
DPMAC3@xgmii |
10G MAC3 USXGMII port |
| 10G MAC4 |
DPMAC4@xgmii |
10G MAC4 USXGMII port |
| 25G MAC5 |
DPMAC5@25g-aui |
25G MAC5 SFP port |
| 25G MAC6 |
DPMAC6@25g-aui |
25G MAC6 SFP port |
| 1G MAC17 |
DPMAC17@rgmii-id |
1G MAC17 RGMII port |
| 1G MAC18 |
DPMAC18@rgmii-id |
1G MAC18 RGMII port |