LS1088ARDB/LS1088RDB-PB Ethernet port mapping

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1088ARDB/LS1088RDB-PB Ethernet port mapping

LS1088ARDB/LS1088RDB-PB Ethernet port mapping

In the U-Boot log, the names of the Ethernet interfaces are printed in the format <name>@<interface type>, for example, DPMAC2@xgmii. DPMAC is a DPAA2 object that identifies the physical interface. 

For Linux, in TinyDistro as well as in Ubuntu distribution, by default, only one MAC is enabled as a standard Kernel Ethernet Interface. This interface is named eth0 by default (or eth1 if PCI Express network interface card is discovered first).

For details regarding creation of a DPAA2 network interface (DPNI) in Linux, refer to LS1088ARDB/LS1088ARDB-PB - How to create a DPAA2 network interface (DPNI) in Linux

The table below shows the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux for LS1088ARDB. 

Port name on chassisPort name in U-BootPort name in Linux (tinyDistro and Ubuntu
userland)
Description
ETH0DPMAC2@xgmiinot enabled by defaultXFI optical interface
ETH1DPMAC1@xgmiinot enabled by defaultXFI copper interface
ETH2DPMAC7@qsgmii not enabled by defaultQSGMII copper
interface
ETH3DPMAC8@qsgmii not enabled by defaultQSGMII copper
interface
ETH4DPMAC9@qsgmii not enabled by defaultQSGMII copper
interface
ETH5DPMAC10@qsgmii not enabled by defaultQSGMII copper
interface
ETH6DPMAC3@qsgmii not enabled by defaultQSGMII copper
interface
ETH7DPMAC4@qsgmii not enabled by defaultQSGMII copper
interface
ETH8DPMAC5@qsgmii eth0 by default (or eth1 if PCI Express network interface card is discovered first)QSGMII copper
interface
ETH9DPMAC6@qsgmii not enabled by defaultQSGMII copper
interface

The table below shows the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux for LS1088ARDB-PB.

Port name on chassisPort name in U-BootPort name in Linux (tinyDistro and Ubuntu
userland)
Description
DPMAC1DPMAC1@xgmiinot enabled by defaultXFI optical interface
DPMAC2DPMAC2@xgmiinot enabled by defaultXFI copper interface
DPMAC3DPMAC3@qsgmiinot enabled by defaultQSGMII copper
interface
DPMAC4DPMAC4@qsgmiinot enabled by defaultQSGMII copper
interface
DPMAC5DPMAC5@qsgmiieth0 by default (or eth1 if PCI Express network interface card is discovered first)QSGMII copper
interface
DPMAC6DPMAC6@qsgmiinot enabled by defaultQSGMII copper
interface
DPMAC7DPMAC7@qsgmiinot enabled by defaultQSGMII copper
interface
DPMAC8DPMAC8@qsgmiinot enabled by defaultQSGMII copper
interface
DPMAC9DPMAC9@qsgmiinot enabled by defaultQSGMII copper
interface
DPMAC10DPMAC10@qsgmiinot enabled by defaultQSGMII copper
interface
标签 (1)
无评分
版本历史
最后更新:
‎10-31-2018 12:24 AM
更新人: