The table below shows the mapping of the Ethernet port names appearing on the front panel of the LS1046ARDB chassis with the port names in U-Boot, tinyDistro, and NXP LSDK userland.
Port name on chassis | Port name in U-Boot | Port name in Linux (tinyDistro) | Port name in Linux (LSDK userland) |
---|
RGMII1 | FM1@DTSEC3 | eth0 | fm1-mac3 |
RGMII2 | FM1@DTSEC4 | eth1 | fm1-mac4 |
SGMII1 | FM1@DTSEC5 | eth2 | fm1-mac5 |
SGMII2 | FM1@DTSEC6 | eth3 | fm1-mac6 |
10G Copper | FM1@TGEC1 | eth4 | fm1-mac9 |
10G SEP+ | FM1@TGEC2 | eth5 | fm1-mac10 |