LS1028 Felix Switch Configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1028 Felix Switch Configuration

LS1028 Felix Switch Configuration

On successful probing of the DSA Felix switch, each available front panel switch port should have a network device interface attached with the swpX name format. The ip link show command uses the swpX@enoY name format to also indicate the associated master Ethernet interface for the DSA switch port, which corresponds to an internal ENETC interface, usually the eno2 (Port2) for the LS1028A SoC.

LS1028 Interface naming in Linux

Single port mode

Bridge mode

附件
评论

useful

100% 有帮助 (4/4)
版本历史
最后更新:
‎10-14-2020 02:20 AM
更新人: