WinUSB driver installation (LPC18xx/LPC43xx)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

WinUSB driver installation (LPC18xx/LPC43xx)

WinUSB driver installation (LPC18xx/LPC43xx)

This procedure no longer applies to DFUSec/LCT. As of v2.00 of the LCT, you no longer need to manually install .NET or the WinUSB driver package - the LCT installer will do that for you if it already isn't installed. WinUSB only needs to be installed on Windows XP machines - it is already part of Win 7/8. All you need to do is download and install the LCT.

To install the WinUSB drivers for the LPC18xx/43xx boards, first configure the board for USB boot. Plug in the USB connector to the board (add external power to the board if necessary) and a new USB device (LPC) should appear.

winusb_inst1.png

Download the drivers at http://www.lpcware.com/content/nxpfile/lpc18xx43xx-winusb-drivers-dfu-boot

Un-compress the drivers and point the driver installation dialog to the INF file in the uncompressed package. After installation is complete, you should have a new device available for the LPC18xx or LPC43x.

winusb_inst3.png

winusb_inst4.png

添付
コメント

Hi,

WinUSB driver is working for windows 7 not for windows 10.

can you please suggest winUSB (LPC 18xx) driver for windows 10??

Thanks,

Hari.

評価なし
バージョン履歴
最終更新日:
‎04-25-2016 02:52 PM
更新者: