Another simple SWIM example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Another simple SWIM example

Another simple SWIM example

Attached is another simple SWIM demo that setups a 240x320 window and draws an animated diamond in the window as fast as possible. Although the code is meant to be used with the LPC32x0 CDL, it can be easily ported to other devices. The code for setting up the window and doing the animations is below:

/* Create a SWIM window */
swim_window_open(&win1, LCD_DISPLAY.pixels_per_line,
    LCD_DISPLAY.lines_per_panel, fblog1, 0, 0,
    (LCD_DISPLAY.pixels_per_line - 1),
    (LCD_DISPLAY.lines_per_panel - 1), 3, WHITE, BLACK, MAGENTA);

    xf = 20;
    yf = 30;
    xinc = 1;
    yinc = 1;
    clr = RED | GREEN;

    /* Draw as fast as possible, no throttling */
    while (1)
    {
       swim_set_fill_color(&win1, clr);
       swim_put_diamond(&win1, LCD_DISPLAY.pixels_per_line / 2,
       LCD_DISPLAY.lines_per_panel / 2, xf, yf);
       lcd_ioctl(lcddev, LCD_SET_UP_FB, PHY_LCD_FRAME_BUF1);

       xf += xinc;
       if ((xf < 10) || (xf > 150))
           xinc = -xinc;
       yf += yinc;
       if ((yf < 10) || (yf > 230))
           yinc = -yinc;

       clr++;
       if (clr > 0xFFFF)
           clr = RED | GREEN;
    }

The file also includes a pre-built image of the program for use with the Phytec LPC3250 board using S1L. To use the image, just boot the board to the S1L prompt, type "load term srec', send the SREC file to the board via the serial port (no transfer protocol), and then type 'exec' to start it.

No ratings
Version history
Last update:
‎04-25-2016 04:49 PM
Updated by: