nxp plain expand devices in the cortex M0?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

nxp plain expand devices in the cortex M0?

10,471 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by thinkchip on Wed Dec 29 23:12:56 MST 2010
Hi, I want to know if NXP have some plan to expand the devices for cortex M0, like 3 uarts, usb, rtc,more pins, etc, thanks
0 项奖励
回复
29 回复数

10,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sat Mar 05 11:59:42 MST 2011
Damned expensive, too :mad::mad:
0 项奖励
回复

10,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larryvc on Sat Mar 05 11:36:30 MST 2011
I like the Fujitsu part for its very low active and standby current. I didn't find stock for this either.

I have been looking at the Ramtron FM24W256.  It seems to fit my requirements also is 256 Kb.

http://www.ramtron.com/files/datasheets/FM24W256_ds.pdf
0 项奖励
回复

10,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sat Mar 05 02:11:01 MST 2011

Quote: larryvc
Zero what is the part number of the FRAM Santa brought you?



It's a Fujitsu MB85RC128 (MB85RC128PNF-G-JNE1). Unfortunately Santa bought the whole stock :mad:
[INDENT]Farnell Order Code: 1831995
[/INDENT][INDENT]Availability: Awaiting Delivery

Datasheet: http://www.semiconductorstore.com/pdf/newsite/Fujitsu/e513110.pdf
[/INDENT]Description:
[INDENT]FRAM: 128Kbit
Voltage Range: 2.7V to 3.6V
Case Style: SOP8
Interface: I2C
Memory Configuration: 16K x 8bit
Operating Temperature Range: -40°C to +85°C
[/INDENT]
0 项奖励
回复

10,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larryvc on Fri Mar 04 22:12:01 MST 2011

Quote: Zero
BTW EEPROM:
Last Christmas (= last week) Santa brought me a FRAM (128K)



Zero what is the part number of the FRAM Santa brought you?
0 项奖励
回复

10,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Jan 12 15:56:18 MST 2011

Quote: NXP_USA
...should be available...



Found a 'Development' product status on NXP website. :(

Is there a roadmap for 'Production' ?
(Just to know if I have to add it to Christmas list 2011 or later...)
0 项奖励
回复

10,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Wed Jan 12 10:34:49 MST 2011
The parts should be available through all of our distributors. There are no plans to limit the sale just to automotive companies.

-NXP
0 项奖励
回复

10,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Jan 12 07:28:20 MST 2011
Yes, it does. Always thought it's not very clever to integrate transceivers, but the more interesting question for me is:
will these wonderful things be available (in small quantities :)) for me through my german distributors or is this stuff just sold to automotive companies :mad:
0 项奖励
回复

10,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ktownsend on Wed Jan 12 07:15:26 MST 2011
Zero:

Thought this might interest you: http://www.electronics-eetimes.com/en/nxp-launches-industry-s-first-integrated-mcu-and-can-transceiv...

LPC11xx with integrated CAN transceiver.
0 项奖励
回复

10,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Jan 04 00:50:02 MST 2011
C library related information can be found at:
http://support.code-red-tech.com/Cod...edFAQ#CLibrary

You might also want  to check that when building a Debug build of your project has the linker option "[FONT=Courier New][SIZE=1]--gc-sections[/SIZE][/FONT]" specified - which will cause unused functions to be eliminated from your final image, and can dramatically reduce overall code size. Some earlier versions of LPCXPresso IDE had this option removed (as did some versions of the example projects).

Anyway, can I suggest that if you want to discuss application size further, then you create a new forum thread - as code size is not really related to the main subject of this thread.

Regards,
CodeRedSupport
0 项奖励
回复

10,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Senso on Mon Jan 03 19:13:35 MST 2011
So, where can I get the newLib and where to put it so the CodeRed IDE can use it?
0 项奖励
回复

10,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cyberstudio on Mon Jan 03 14:41:03 MST 2011
Adding to the list of wants, I want smaller than LQFP64. ST is able to jam 64 pins into a 5mm x 5mm BGA and NXP could easily do the same, after all they are the one coming up with the 2mm x 2mm LPC1102.
0 项奖励
回复

10,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Jan 03 09:38:48 MST 2011

Quote: KTownsend
You wanted RTC ... they gave it to you. You should have told Santa that you ALSO wanted CAN. :p Now you'll have to wait until next Christmas for better presents.



Come on, don't blame Santa :)
He knows for sure that we always want more and more features and not less.
Unfortunately someone else :confused: must have forgotten to invite him to this roadmap meetings.
0 项奖励
回复

10,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ktownsend on Mon Jan 03 08:20:21 MST 2011

Quote: Zero
Q1, that's now :)
Is there a roadmap for releasing an UM?
NXP Search doesn't show results.
Found a preliminary at
http://www.zlgmcu.com/NXP/LPC1000/LPC1200/LPC122x_UM_EN.pdf
LQFP64 and no CAN :confused:



You wanted RTC ... they gave it to you.  You should have told Santa that you ALSO wanted CAN.  :p  Now you'll have to wait until next Christmas for better presents.

I've actually been looking at the 122x and it's kind of a tradeoff for me.  The speed is fine (though a bit limited with the internal crystal), and I really need the extra flash space and the RTC (at last!) ... but with more pins than the 1114 only one SSP block kind of stinks.  I often need two since I like to have a dedicated SPI block for the radio transceiver and a second one for an SD card or an external 16-bit ADC or high-traffic sensor, etc.

I'm going to use it for a wireless protocol analyser (for debugging 802.15.4 traffic), but it's not really an upgrade to the 1114/1343 per se.  It has some things I miss in the 1100/1300 family (more flash + RTC), but you lose a few things I would have found useful (two SSPs and maybe CAN).

There are some pretty cool new peripheral blocks though that look really interesting and useful ... but I don't really want to list a lot of details until a UM is published somewhere officially.  It looks like an interesting chip and I'm looking forward to trying it, I just wouldn't really consider it an upgrade to the 1114 ... it's kind of a different mix of features.  Hope the price is as competitive at the 1100s though.
0 项奖励
回复

10,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Jan 03 05:38:49 MST 2011
Q1, that's now :)
Is there a roadmap for releasing an UM?
NXP Search doesn't show results.
Found a preliminary at
http://www.zlgmcu.com/NXP/LPC1000/LPC1200/LPC122x_UM_EN.pdf
LQFP64 and no CAN :confused:
0 项奖励
回复

10,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Mon Jan 03 03:12:27 MST 2011
[COLOR=black][FONT=Arial][/FONT][/COLOR]
[COLOR=black][FONT=Arial]The roadmap has the LPC122x on it, which has a RTC and 128KB of Flash.[/FONT][/COLOR]
[COLOR=black][FONT=Arial]This part will be released in Q1 2011.[/FONT][/COLOR]
0 项奖励
回复

10,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Sun Jan 02 09:36:29 MST 2011
You might find optimizing for space improves your code size still further. The normal optimization levels (O1, O2, O3) are for performance optimizations, which can  *increase* code size (especially between O2 and O3 because the compiler will do things like loop unrolling etc).

In Code Red, you will need to add -Os in the "Other optimisations" box.

HTH
0 项奖励
回复

10,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Wenzu on Sat Jan 01 19:53:49 MST 2011

Quote:
A simple 4 interrupt capture is swallowing 20K of code !!! :confused:

My mistake. I had UART + I2C enabled.

So.. took advice given earlier..and re-compiled to see differences.

a simple 4 input capture using 2x 32-Bit timers and 2x 16-Bit Timers just capturing only... no other stuff, no printf etc... 8388 ( text )

If I optimize at level 03, it goes down to 6996  ( text )

( text )  I am assuming is the code size after a compile.....

OK.. I am now reading AN10963.pdf to better understand what needs to be done.
0 项奖励
回复

10,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sat Jan 01 18:23:08 MST 2011

Quote:
I'm not sure what you're doing to get 20KB code for something seemingly simple? I had FAT32/SDHC + a 240x320 TFT LCD + USBCDC + a command-line interface and ~20 commands and drivers for things like EEPROM, etc., plus a decent graphics library with embedded fonts compiling in around 28KB flash. 32KB is tight, but you can still do a lot with it with careful programming.


BTW EEPROM:
Last Christmas (= last week) Santa brought me a FRAM (128K) :).
So I threw good old 512K EEPROM away and made a few tests:
>12 times faster and working with standard I2C driver without problems. :D
0 项奖励
回复

10,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sat Jan 01 18:05:00 MST 2011
SO20, they must be kidding :)
0 项奖励
回复

10,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ktownsend on Sat Jan 01 17:19:27 MST 2011

Quote: Wenzu
Ditto for me....

I am disappointed today, because ( as a 1343/ARM noob ) I have discovered that 32k is being filled up with only barebones code....
A simple 4 interrupt capture is swallowing 20K of code !!! :confused:
Main code is already 20K alone....



I'm not sure what you're doing to get 20KB code for something seemingly simple?  I had FAT32/SDHC + a 240x320 TFT LCD + USBCDC + a command-line interface and ~20 commands and drivers for things like EEPROM, etc., plus a decent graphics library with embedded fonts compiling in around 28KB flash.  32KB is tight, but you can still do a lot with it with careful programming.

Try compiling with -0s and in release mode, for example?
0 项奖励
回复