download application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

download application

230件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mawpe on Thu Oct 25 02:39:28 MST 2012
Hey

Is there a PC program besides LPCXpresso, where I can download a app to a target board via LPC-Link?

Or is there a way to use LPCXpresso to download a app, when you only have a bin or hex file?

Thank you!
0 件の賞賛
返信
1 返信

224件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Oct 25 02:52:50 MST 2012

Quote:

Is there a PC program besides LPCXpresso, where I can download a app to a target board via LPC-Link?

FlashMagic via ISP-UART:

http://www.support.code-red-tech.com/CodeRedWiki/OutputFormats?highlight=%28flashmagic%29


Quote:

Or is there a way to use LPCXpresso to download a app, when you only have a bin or hex file?

Flash-Tool:

http://www.support.code-red-tech.com/CodeRedWiki/GuiFlashProgramming?highlight=%28flash%29

There's also a command line version of Flash-Tool:

http://www.support.code-red-tech.com/CodeRedWiki/CommandLineFlashProgramming
0 件の賞賛
返信