connection problem with OM13085

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

connection problem with OM13085

1,595 次查看
prasadkadam
Contributor I

Hi

 I am facing problem while connecting the OM13085 with laptop, am using LPCExpresso with open-suse  42.3 Leap version.i checked for the Dmseg for errors and found that a problem stating "cant add hid device: -110"

adding the snippets from my Dmesg.(the board uses LPC1769)

                          usb 1-6: new full-speed USB device number 8 using xhci_hcd
[ 3687.658513] usb 1-6: New USB device found, idVendor=1fc9, idProduct=001d
[ 3687.658515] usb 1-6: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 3687.658516] usb 1-6: Product: NXP CMSIS-DAP
[ 3687.658518] usb 1-6: Manufacturer: NXP
[ 3707.655956] usbhid 1-6:1.0: can't add hid device: -110
[ 3707.655981] usbhid: probe of 1-6:1.0 failed with error -110

Best Wishes!

0 项奖励
回复
2 回复数

1,402 次查看
prasadkadam
Contributor I

hi

            Thank you for the reply Brendon , I am using Open-suse leap as my Os as mentioned earlier.

  and i think the drivers u referred are for windows.but open-suse is a Linux flavor.so still the problem persists.

Regards,

Prasad

 

0 项奖励
回复

1,402 次查看
brendonslade
NXP TechSupport
NXP TechSupport

Hi Prasad,

The first OM13085 boards shipped used mbed-based debug probe firmware (note this board is not Mbed-enabled). Latest versions use an firmware version, which can be found here:

https://www.nxp.com/webapp/sps/download/license.jsp?colCode=LPC11Uxx-Debug-Probe-VCOM

You haven't stated what OS you are running. Windows? If so, the driver included in this package will be needed for Windows 7 or 8.

Please try unplugging your board, installing this driver, and trying again ... We'd appreciate it if you can let us know if this works.

Regards,

Brendon

0 项奖励
回复