arm-none-eabi-gdb.exe has stopped working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

arm-none-eabi-gdb.exe has stopped working

559 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by erbal_gfx on Tue Jul 14 00:59:48 MST 2015
Hello Guys!

I've discovered a strange thing in LPCXpresso v7.0.0 [Build 92] [2014-02-20] (on Windows 7). My problem is the following:
[list=1]
  [*]My project is working, I can debug my code. Everything works fine.
  [*]I can build the project, it is even downloaded into the controller but I cannot debug my code because "arm-none-eabi-gdb.exe has stopped working" (LPC1549 in this case, but I've experienced this with LPC1769 too).
  [*]I create a new project, import the old one, which failed at debug. I start a debug session and it works fine again. The interesting part is if I deleted the old project and rename the new one to the old one's name. It fails at debug again. That's why I think some project or meta files are stucked in the project somehow.
[/list]


Is there a solution to bypass this create new project, import the old one, delete the old one part? It kills my version controlling.

0 项奖励
回复
1 回复

489 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Jul 14 01:05:41 MST 2015
Almost certainly this is because you have breakpoints set on unused code (code that is being discarded by the linker as it is not used).

If this happens:
- delete ALL of your breakpoints (do it from the Breakpoints view) and then try again
- upgrade to latest version, where this is improved (but not yet fixed)
0 项奖励
回复