We are using LPC1769 board for our Smart Card Reader IC (IC CLRC663 and Mifare Classic 1K card).
Attached link for Xpresso Board:
https://www.embeddedartists.com/sites/default/files/docs/schematics/LPCXpresso1769_CD_revD.pdf
We want to connect JTAG debugger Keil uLink2 or uLink Pro D to LPCXpresso1769 CMSIS-DAP rev-D board. (since both debugger are available with us). I have 3 queries regarding JTAG interface.
1) Can we use above debuggers (Keil uLink2 or uLink Pro D) with Xpresso dev board (LPCXpresso1769 CMSIS-DAP)
2) It is mentioned in schematics that by providing shortlink to JP3, CMSIS-DAP is disabled and external debugger can be connected. Is it correct or any other hardware setting needs to be done to connect JTAG Debugger?
3) If no, which JTAG debugger can be used for Xpresso IDE ?
Please advise. Thanks in advance.
Details of LPCXpresso IDE support for CMSIS-DAP based debug probes can be found at:
CMSIS-DAP support in LPCXpresso
More general information on debug probe support with LPCXpresso IDE can be found at:
https://community.nxp.com/message/630901
If you want to use an external probe with your LPCXpresso1769-CD board, then I would suggest looking at the LPC-Link2 probe, which was designed explicitly for LPCXpresso IDE use, and which provides additional functionality when used with LPCXpresso IDE - in particular SWO Trace capabilities.
Regards,
LPCXpresso Support
Thanks Con Verse for reply, which probe you are talking about? Do you mean uLink 2 or Ulink Pro D?