Red Probe+ compatibility with LPCXpresso v7.3.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Red Probe+ compatibility with LPCXpresso v7.3.0

624 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Tom Barrett on Thu Aug 28 08:10:43 MST 2014
I have a Red Probe+ USB debug probe that is a couple of years old but was never used with Code Red tools of the same vintage. I have returned to the project but am now using LPCXpresso v7.3.0 (free edition because of the small project size). Does this version of LPCXpresso support the Red Probe+ and my target, which is a Cortex-M0 LPC1227-SK board from IAR.

Thanks for the help.
0 Kudos
Reply
3 Replies

609 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by liana on Sun Aug 31 22:57:10 MST 2014
I agree with this...
0 Kudos
Reply

609 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Tom Barrett on Fri Aug 29 13:33:18 MST 2014
Great! Thanks for the quick reply.

TB
0 Kudos
Reply

609 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Aug 28 08:38:23 MST 2014
Yes to both questions.
0 Kudos
Reply