No connection to emulator device?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No connection to emulator device?

1,420 Views
raphaelprechtel
Contributor I

Hello,

I am using the NHS 3152 on the Eval-board "NHS3152THADADK", which has 13 switches. I changed the blinky demo software to get an output at GPIO 5 and 7. The other Pins I wanted to use as Inputs, to see whether I can detect my output signal on an Input pin, because of the internal connection caused by the switches.

After flashing my program I am not able anymore to connect to the microcontroller. I attached the code and the error message.

Somehow I think it was a bad idea to change the programming pins 10 and 11 to Input and that's why I can't connect to the core anymore.

I hope someone can help me.

Greetings,

Raphael

0 Kudos
0 Replies