Content originally posted in LPCWare by cbarberis on Tue Mar 10 08:19:35 MST 2015
Hi
I am brand new to the ARM family and I just purchased the LPCxpresso LPC1769 board and downloaded many of the project files associated with it. However, the only example program I find is "Freertos blinky" which blinks a LED on the board. I am just interested in the simplest type of example program without any RTOS involved, in other words a simple program that I can easily manipulate and learn from. Is there such a thing as just a "Blinky" program without the rots that I can load as a project for the above board. Any other simple source code examples for this board would also work just as well. Any advice would be greatly appreciated.