Led blinky SDK for my LPCXpresso 824 Max board.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Led blinky SDK for my LPCXpresso 824 Max board.

Jump to solution
2,700 Views
ooooowen
Contributor I

Hello , I have tried to modify the led_blinky demo code to blink the GREEN LED for a month.

But even I modified all the functions about LED in the main function, It still doesn't work.

The demo code version is SDK_2_9_0_LPCXpresso824MAX-lpcxpresso824max_led_blinky

Those functions that I have been modified are

======================================

pin_mux.c - BOARD_InitPins 

add

const uint32_t IOCON_INDEX_PIO0_16_config = (/* Selects pull-up function */
IOCON_PIO_MODE_PULLUP |
/* Enable hysteresis */
IOCON_PIO_HYS_EN |
/* Input not invert */
IOCON_PIO_INV_DI |
/* Disables Open-drain function */
IOCON_PIO_OD_DI |
/* Bypass input filter */
IOCON_PIO_SMODE_BYPASS |
/* IOCONCLKDIV0 */
IOCON_PIO_CLKDIV0);

IOCON_PinMuxSet(IOCON, IOCON_INDEX_PIO0_16, IOCON_INDEX_PIO0_16_config);

======================================

pin_mux.h

add

#define BOARD_LED_GREEN_PERIPHERAL GPIO /*!<@brief Device name: GPIO */
#define BOARD_LED_GREEN_SIGNAL PIO0 /*!<@brief GPIO signal: PIO0 */
#define BOARD_LED_GREEN_GPIO GPIO /*!<@brief GPIO device name: GPIO */
#define BOARD_LED_GREEN_GPIO_PIN 16U /*!<@brief PIO0 pin index: 12 */
#define BOARD_LED_GREEN_PORT 0U /*!<@brief PORT device name: 0U */
#define BOARD_LED_GREEN_PIN 16U /*!<@brief 0U pin index: 12 */
#define BOARD_LED_GREEN_CHANNEL 16 /*!<@brief GPIO PIO0 channel: 12 */
#define BOARD_LED_GREEN_PIN_NAME PIO0_16 /*!<@brief Pin name */
#define BOARD_LED_GREEN_LABEL "SW2/D1[1]/P3[45]/J2[5]/P0_12-RED-ISP" /*!<@brief Label */
#define BOARD_LED_GREEN_NAME "LED_GREEN" /*!<@brief Identifier name */
#define BOARD_LED_GREEN_DIRECTION kPIN_MUX_DirectionOutput /*!<@brief Direction */

======================================

Led_blinky.c

#define BOARD_LED_PORT BOARD_LED_GREEN_PORT
#define BOARD_LED_PIN BOARD_LED_GREEN_PIN

======================================

LPC824.h(Both of them aren't work)

/*
#define IOCON_INDEX_PIO0_17 (0 )
#define IOCON_INDEX_PIO0_13 (1 )
#define IOCON_INDEX_PIO0_12 (2 )
#define IOCON_INDEX_PIO0_5 (3 )
#define IOCON_INDEX_PIO0_4 (4 )
#define IOCON_INDEX_PIO0_3 (5 )
#define IOCON_INDEX_PIO0_2 (6 )
#define IOCON_INDEX_PIO0_11 (7 )
#define IOCON_INDEX_PIO0_10 (8 )
#define IOCON_INDEX_PIO0_16 (9 )
#define IOCON_INDEX_PIO0_15 (10)
#define IOCON_INDEX_PIO0_1 (11)
#define IOCON_INDEX_PIO0_9 (13)
#define IOCON_INDEX_PIO0_8 (14)
#define IOCON_INDEX_PIO0_7 (15)
#define IOCON_INDEX_PIO0_6 (16)
#define IOCON_INDEX_PIO0_0 (17)
#define IOCON_INDEX_PIO0_14 (18)
#define IOCON_INDEX_PIO0_28 (20)
#define IOCON_INDEX_PIO0_27 (21)
#define IOCON_INDEX_PIO0_26 (22)
#define IOCON_INDEX_PIO0_25 (23)
#define IOCON_INDEX_PIO0_24 (24)
#define IOCON_INDEX_PIO0_23 (25)
#define IOCON_INDEX_PIO0_22 (26)
#define IOCON_INDEX_PIO0_21 (27)
#define IOCON_INDEX_PIO0_20 (28)
#define IOCON_INDEX_PIO0_19 (29)
#define IOCON_INDEX_PIO0_18 (30)
*/

#define IOCON_INDEX_PIO0_13 (1 )
#define IOCON_INDEX_PIO0_12 (2 )
#define IOCON_INDEX_PIO0_5 (3 )
#define IOCON_INDEX_PIO0_4 (4 )
#define IOCON_INDEX_PIO0_28 (5 )
#define IOCON_INDEX_PIO0_3 (6 )
#define IOCON_INDEX_PIO0_2 (7 )
#define IOCON_INDEX_PIO0_11 (8 )
#define IOCON_INDEX_PIO0_10 (9 )
#define IOCON_INDEX_PIO0_16 (10)
#define IOCON_INDEX_PIO0_27 (11)
#define IOCON_INDEX_PIO0_26 (12)
#define IOCON_INDEX_PIO0_25 (13)
#define IOCON_INDEX_PIO0_24 (14)
#define IOCON_INDEX_PIO0_15 (15)
#define IOCON_INDEX_PIO0_1 (16)
#define IOCON_INDEX_PIO0_9 (17)
#define IOCON_INDEX_PIO0_8 (18)
#define IOCON_INDEX_PIO0_7 (22)
#define IOCON_INDEX_PIO0_6 (23)
#define IOCON_INDEX_PIO0_0 (24)
#define IOCON_INDEX_PIO0_14 (25)
#define IOCON_INDEX_PIO0_23 (26)
#define IOCON_INDEX_PIO0_22 (27)
#define IOCON_INDEX_PIO0_21 (28)
#define IOCON_INDEX_PIO0_20 (29)
#define IOCON_INDEX_PIO0_19 (30)
#define IOCON_INDEX_PIO0_18 (31)
#define IOCON_INDEX_PIO0_17 (32)

======================================

Could anyone tell me where did I make mistakes?

Thanks a lot

0 Kudos
1 Solution
2,682 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

 

GPIO out put direction and function:

Alice_Yang_0-1626850102622.png

 

View solution in original post

4 Replies
2,694 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ooooowen,

I modify it for you, the GREEN led can work well, please see my attachment project. 

 

Hope it helps,

Alice

0 Kudos
2,692 Views
ooooowen
Contributor I

Thanks, it does work. I'm sorry, could you tell me what's different about tour project and mine? except IOCON_INDEX_PIO0_16 and BOARD_LED_PIN

I trying to the BLUE LED by modify those two defines , but it's the same situation with my previous question.

0 Kudos
2,683 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

 

GPIO out put direction and function:

Alice_Yang_0-1626850102622.png

 

2,672 Views
ooooowen
Contributor I

Got it. Thank you.

0 Kudos