Customer wants to use LPCXpresso for cost down. I have looked the picture following.
NGX Xplorer LPC4330 Board only support Redlink. That’s reason why function can’t work fine after I use LINK-II to program code into QSPI Flash.
I try to use NXP LPCXpresso4337 to download to NGX Xplorer LPC4330 Board.
The result is I’m failed to download code to QSPI Flash.
There is no way for customer to use LPCXpresso IDE and LINK-II right?
If yes, what’s Redlink debugger and can let customer use LPCXpresso IDE.
Or customer can only use Keil C to develop LPC4330?
That page appears to be out-of-date. There is no problem using a CMSIS-DAP probe, such as LPC-Link2, to debug an LPC4330 from LPCXpresso IDE. For more information, please see: Which debug probes are supported by LPCXpresso IDE with which MCUs?
Regards,
LPCXpresso Support