Dear Ladies and Gentlemen,
I have following software installed:
-LPCXpresso V8.2.2 [Build 650]
-Eclipse plugin: com.nxp.pn7xxxxx.update-8.0.0-SNAPSHOT-155.zip
When I click on "Program Flash" in the toolbar of LPCXpresso it connects succesfully to the emulator (LPC-LINK 2) and after connection following error are output:
-
LPCXpresso: Exception
CoreException
Reason:
Plug-in com.crt.vendor.nxp.pn7xxxxx was unable to load class
com.crt.vendor.nxp.pn7xxxxx.support.FlashDialogFactoryPn7xxxxx.
-
What am I doing wrong, which package is missing?
Thank you very much.
Best Regards
Stefan Mueller
You may also be able to use the command line flash programmer, as described in :https://community.nxp.com/message/630785
Regards,
LPCXpresso Support
This works. But it is a little bit annoying. I would appreciate it, if you can provide the ..SNAPSHOT-163.zip.
Best Regards
Stefan
Hi Stefan,
new package will be availble in next weeks, this package will also contain new plugin.
In case you need it before, please provide an email where I can send it.
Kind Regards,
Mirjan.
Thank you. I will wait.
Till now we are in the evaluating phase, which controller we are going to use in future for our products.
Best Regards
Stefan
Hi Stefan,
by my Information you already got the new PN7462 plugin for the LPCXpresso, Version "com.nxp.pn7xxxxx.update-8.0.0-SNAPSHOT-163.zip". This plugin should solve the issue.
Plugin will be available with next release (part of the release package), according to the plan this will be at beginning of the next year.
Dear Mirjan,
thank you for your reply.
I don't have the plugin. Could you please tell me how I can get it? Do I have to wait for official release?
Best Regards
Stefan