Content originally posted in LPCWare by jedrzej.dudkiewicz on Thu Nov 13 04:34:26 MST 2014
Well, I don't know about it. I see in registry that there is key "HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Microsoft\Windows\CurrentVersion\Uninstall\LPCXpresso7_is1", which is pretty generic if you ask me, there is no version number or anything else in the name. But yeah, I don't suppose any value kept there should apply to debugging or building. On the other hand this is info for uninstaller, so maybe when I removed an old version something went wrong. If I recall correctly I uninstalled 7.3 using unins000.exe in installation directory - maybe it was bad thing to do.
Never the less without full reinstall of 7.5 I were unable to compile single file. I've been creating new workspaces, deleting various configuration files in existing ones (actually in copies of workspaces) to no avail.
Anyway, now that I think about it it's probably a problem with LPCXpresso's base, that is Eclipse/CDT tandem, so it wasn't the best place to ask this question to begin with. Sorry.