LPCXpresso 1343 board fails to connect with JTAG debugger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso 1343 board fails to connect with JTAG debugger

1,018件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embedsoft on Mon May 31 00:54:39 MST 2010
Hi all,

My LPCXpresso 1343 board fails to connect with the JTAG debugger.
I have searched the LPCXpresso knowledgebase, but that didn't resolve my problem.:mad:
I get the following error pop-up window when trying to program the flash memory by means of the Xpresso IDE v3.3.4.

Errors from: 'crt_emu-lpc11_13-nxp -pLPC1343 -info-clock'
Premature end of file,Ni:
LPCXpresso Debug driver v2.0
Et: Failed emulator initialization: E(xx)
FTDI driver load/install error, ftd2xx.dll

Any help I will be highly appriciate!

embedsoft
0 件の賞賛
返信
3 返答(返信)

1,009件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sat Jun 05 07:17:58 MST 2010
You appear to be encountering a similar problem to that in the following forum thread...

http://knowledgebase.nxp.com/showthread.php?t=380

And the fact that you see a reference in the error box to FTDI does indicate that the debugger is at this point looking for the Red Probe driver (which should be installed during the LPCXpresso IDE installation process - as long as, if prompted, you allow it).

Can you confirm that if you click on OK in the error box, you then successfully connect to the board?

Regards,
CodeRedSupport
0 件の賞賛
返信

1,009件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embedsoft on Sat Jun 05 01:17:31 MST 2010

Quote: CodeRedSupport
It looks like it is missing a device driver.

Did you allow the device drivers to install when you installed the LPCXpresso? Can you try reinstalling and make sure the drivers install.



I reinstalled the LPCXpresso IDE, but the problem still exists.
Is there anything else I can do to restore?

embedsoft
0 件の賞賛
返信

1,009件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon May 31 01:32:19 MST 2010
It looks like it is missing a device driver.

Did you allow the device drivers to install when you installed the LPCXpresso? Can you try reinstalling and make sure the drivers install.
0 件の賞賛
返信