the LPC4088 QSB card is working correctly when using mbedCompiler (programming software / reset / soft working correctly).
when i connect EmbeddedArtists LPC4088 QSB Card + LPCXPRESSO V8.2.2 + LPCLINK2, the following failure appears on console debug message when trying connection with debugger :
" LPCXpresso RedlinkMulti Driver v8.2 (Sep 5 2016 10:12:38 - crt_emu_cm_redlink build 725)
Found chip XML file in C:/Users/preyg/Documents/LPCXpresso_8.2.2_650/workspace/lwip_tcpecho_freertos/Debug/LPC4088.xml
Failed on connect: Ee(36). Could not connect to core.
No connection to emulator device ".
ERROR REPORTED BY TARGET :
02: Failed on connect
Could not connect to core.
31: No connection to emulator device
i have tried proposed solution on this blog : Regaining debug access to target MCU
using buttons SW1 + SW2 or changing "vector cache", it is still don't work
DO YOU HAVE ANY SOLUTION?
thanks a lot
已解决! 转到解答。
Please try the following..
Now start a debug session for your project, and see what happens.
If you fail to get a debug connection still, please post the full debug log from the console view for us to look at...
https://community.nxp.com/message/630852
Regards,
LPCXpresso Support