LPC Link2 USB PORT RESET FAILED ERROR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC Link2 USB PORT RESET FAILED ERROR

1,081 Views
Sriharsha_Desai
Contributor I

Hi,

Setup: MIMXRT685_EVK_CM33 board

Requirment: To debug / access console from UART from LINK usb. I am using J-Link to flash the program.

Problem: When I connect the EVK to USB of host. I am Not able to debug using LPC LInk2 and the device is not enumerated as COM port. In the device manager getting error as "USB Device PORT Reset Failed"

 

Note: I have updated the LINK usb with latest J-Link firmware using LPCScrypt tool.

How to restore the LPC of the NXP EVK? 

Tags (2)
0 Kudos
Reply
2 Replies

252 Views
chris1058
Contributor I

Hello, @Sriharsha_Desai nystateofhealth

Certainly! To restore the LPC-Link2 on your MIMXRT685_EVK_CM33 board, follow these steps:

Navigate to the root directory where LPCScrypt is installed (e.g., C:\nxp\LPCScrypt\scripts).
Run the program_CMSIS script. This should help resolve the “USB Device PORT Reset Failed” issue. If you continue to face problems, consider contacting NXP TechSupport for further assistance.

I hope this will help you

Best regards

0 Kudos
Reply

1,064 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, 

As same that you changed the firmware for the J-Link, using the LPCScript in root C:\nxp\LPCScrypt\scripts and run program_CMSIS.

Best regards,
Pavel

 

0 Kudos
Reply