LPC Link2 COM port

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC Link2 COM port

6,024件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dalzan on Tue May 17 15:45:50 MST 2016
Hi,
I am a beginner with LPC/ARM.

When I connect LPC Link2 via USB to my computer and launch Debug there appear 2 "HID Standard Devices" / "CMSIS-DAP" and "LPC-SIO Port", and also "Ports (COM and LPT)" / "LPC-LinkII UCom Port (COM3)". Maybe also some others I haven't noticed..

Do I understand right the HID interface is used for JTAG/SWD debugger and the port COM3 is free to use ?
I see on the schematic diagram of Link2 that "Serial Expansion Interface" connector J3 contains pins UART2_RXD + UART2_TXD;
when I open this COM3 with TeraTerm or other UART terminal and enter some text, will it be transmitted to this UART2_TXD ?

I know I could test it myself, problem is with the 50mils fine pitch headers, not so easy to connect anything here quickly.
My plan is to interconnect Link2 (UART2 pins mentioned above) with NGX LPC-4330-Xplorer / connector J8 / pins 9,10 == U0_TXD+U0_RXD.
Then I could test application with UART output without a need for additional TTL->UART->USB converter.

Any comments appreciated.
0 件の賞賛
返信
3 返答(返信)

4,037件の閲覧回数
prakashxd
Contributor I

 VCOM port mostly will solve the issue.

https://mycfavisit.site

0 件の賞賛
返信

4,920件の閲覧回数
Kasey00
Contributor I

HS USB bandwidth and available SRAM was seen as too limiting; ports P2_0 and P2_1 were used as trace testmyspeed.onl port connections to the target via a  buffer. 

0 件の賞賛
返信

5,317件の閲覧回数
brendonslade
NXP TechSupport
NXP TechSupport

The default firmware for the standalone LPC-Link2 uses the same port pins as the on-board version, which are P2_0 and P2_1. When LPC-Link2 was initially designed there was a long term goal to support parallel trace, which was never implement as HS USB bandwidth and available SRAM was seen as too limiting; ports P2_0 and P2_1 were used as trace port connections to the target via a buffer. 

It is possible to get a unidirectional VCOM port (from a target to the host PC via LPC-Link2) by connecting to pin 16 of the SWD/JTAG/ETM connector J8 at pin 16. Due to the buffer between the LPC4370 on LPC-Link2 (originally intended for trace data), it is not possible to get data in the other direction.

0 件の賞賛
返信