Hi,
I've install LPCXpresso v8.2.2 [Build 650] [2016-09-09] in a Windows 10 - 64 bits PC.
When I've connected LPC-Link1 to the USB, LPCExpresso does not recognize it.
I've deleted the driver Driver and then connect the LPC-Link and it had been detected as a DFU device.
Then I've reinstalled the driver from c:\nxp\LPCXpresso_8.2.2_650\Drivers\LPC-Link\ (See Images) but the LPC link driver seems to be not the correct for Win10. After that, LPC Expresso still not recognize it.
Is there another driver version for Windows 10-64 bits ?
I've already probed with 2 different LPC-Link devices and 2 different Mini USB cables.
Urgent response will be appreciated.
Regards,
Gus
I too cannot get my LPCXpresso11u68 recognized on windows 10. Drivers and software installed OK, but nothing is recognized when its connected to the link connector with jumper 1 off, jumper 2&3, and dfu off.
Got it at a ham radio swap fest. It looks handy for use with MBED which I am familiar with.
No connection so the MBED update wouldn't take,
Any help appreciated.
Bo W4GHV
There is no updated LPC-Link driver. We have not seen any issues ourselves using LPC-Link on Windows 10. What is the exact version of Windows that you are using?
In the first place, please run through the FAQ: https://community.nxp.com/thread/388960
Regards,
LPCXpresso Support
Did you try going through the FAQ previously referenced?
Regards,
LPCXpresso Support
Yes, I did.
Still Not working on LPCXpresso 8....