Hello,
I'm using the NHS3152 and want to use the I²C bus. I have tested the example of NXP but it doesn't work. Also I tried my own programm based on the example, which isn't working, too.
Is the programm tested for this chip?
I am not even getting a clock signal at the SCL pin. But perhaps I am doing something completely wrong.
Here is my main:
#include "board.h"
#include "NHS+MAX.h"
#define I2C_MASTER
#ifdef I2C_MASTER
#include "master.h"
#endif
int main(void)
{
if (I2C_SYSTEMCLOCK == NSS_SFRO_FREQUENCY) {
Chip_Flash_SetHighPowerMode(true);
}
Chip_Clock_System_SetClockFreq(I2C_SYSTEMCLOCK);
Board_Init();
#ifdef I2C_MASTER
Master_Init_NHS();
uint32_t MAX_ID;
while (true) {
MasterRead_MAX(0xFF,0x57, (uint8_t*) &MAX_ID, sizeof(MAX_ID));
Chip_Clock_System_BusyWait_ms(I2C_MASTER_COMM_INTERVAL);
printf("%i \n", MAX_ID);
}
#endif
}
I try to read the id of a MAX30101 Sensor.
If someone could help me, that would be great!!
Sincerely,
Raphael